Energy Analysis Dashboard Module operation

NOTE: This module requires a separate license. See Licensing for more information.

The Energy Analysis Dashboard Module includes dashboard gadgets that help you break down consumption by load type, visualize consumption cost, and do an 80/20 analysis to identify the largest consumers. You can identify consumption patterns and anomalies and compare different consumers over time.

Use the Energy Analysis Dashboard Module to:

  • Break down consumption by load type.
  • Visualize consumption cost.
  • Do an 80/20 analysis to identify the largest consumers.
  • Identify consumption patterns and anomalies.
  • Compare different consumers over time.

The following gadgets are part of this module:

  • Aggregated Consumption Ranking gadget
  • Aggregated Pareto Chart gadget
  • Consumption Ranking gadget
  • Heat Map gadget
  • Pareto Chart gadget
  • Sankey gadget

See Gadgets for information on how to use these gadgets.

Related topics:

Energy Analysis Dashboard Module topics

Other Software Modules