Energy Billing Module operation
NOTE: This module requires a separate license. See Licensing for more information.
The Energy Billing Module is a fully functional energy-based billing reporting system. It also provides load and consumption monitoring and reporting at the branch circuit level, which is typically used in data center applications.
Use the Energy Billing Module to:
- Allocate energy costs to consumers.
- Verify utility bills through shadow billing.
- Avoid demand charges.
- Export energy billing data to accounting and financial systems.
- Allocate branch circuit consumption to customers and IT racks.
- Produce energy threshold reports.
- Bill clients for excess energy consumption.
The following reports are part of this module:
- Billing Report
- Billing Summary Report
- Billing Verification Report
- Energy by IT Customer Report
- Multiple Billing Report
- Multiple Billing Export Report
For information on how use the Billing reports (except Energy by IT Customer Report), see Billing Reports
For information on how use the Energy by IT Customer Report, see IT Billing Reports
Related topics:
Energy Billing Module topics
- Energy Billing Module design
- Energy Billing Module configuration
- Energy Billing Module operation
Other Software Modules
- Backup Power Module operation
- Breaker Performance Module operation
- Capacity Management Module operation
- Energy Analysis Dashboard Module operation
- Energy Analysis Reports Module operation
- Event Notification Module operation
- Insulation Monitoring Module operation
- Power Quality Performance Module operation