Insulation Monitoring Module operation
NOTE: This module requires a separate license. See Licensing for more information.
The Insulation Monitoring Module provides monitoring for isolated (IT) power systems, such as the ones found in hospital operating rooms. It also helps in locating isolation faults. The module can be configured for applications based on the IEC standard, and for applications based on the ANSI standard.
Use the Insulation Monitoring Module to:
- Monitor the status of the isolated power system.
- Identify situations when the isolation of the system might be compromised.
The following report and diagrams are part of this module:
- Insulation Monitoring Report (ANSI and IEC)
- Vista diagrams for group, area, and area details levels (ANSI and IEC)
For information on how to use the Insulation Monitoring diagrams and reports, see:
Related topics:
Insulation Monitoring Module topics
- Insulation Monitoring Module Design
- Insulation Monitoring Module configuration
- Insulation Monitoring Module operation
Other Software Modules
- Backup Power Module operation
- Breaker Performance Module operation
- Capacity Management Module operation
- Energy Analysis Dashboard Module operation
- Energy Analysis Reports Module operation
- Energy Billing Module operation
- Event Notification Module operation
- Power Quality Performance Module operation