Configure
This
The
Use the information in the following tables to find the content you are looking for:
Main functions:
| Function | Task |
|---|---|
| Alarms configuration | Configure alarm and incident views in Web Applications. |
| Cybersecurity | Provides recommended actions to help secure your system. |
| Dashboards configuration | Configure Dashboards and Slideshows in Web Applications. |
| Database maintenance | Configure and schedule tasks such as backup, archive, and trim. |
| Diagrams and graphics configuration | Configure Diagrams in Web Applications. |
| Duplicate Data logging | Enable the logging of duplicate historical data records. |
| Licensing configuration | Configure the software and device licenses. |
| Reports configuration | Configure Reports in Web Applications. |
| Software Alarms | Configure Software Alarms. |
| System integration | Integrate PME with other EcoStruxure™ systems. |
| System performance | Customize system parameters to optimize performance. |
| Time synchronization | Configuring time synchronization for monitoring devices. |
| Trends configuration | Configure Trends in Web Applications. |
Software modules:
| Module | Application |
|---|---|
| Backup Power Module configuration |
Generator and Uninterruptible Power Supply (UPS) performance monitoring and reporting, including battery health. |
| Breaker Performance Module configuration |
Circuit breaker aging and breaker settings monitoring. |
| Capacity Management Module configuration |
Generator and Uninterruptible Power Supply (UPS) capacity monitoring and reporting. Includes transformer and UPS loss monitoring. |
| Energy Analysis Dashboard Module configuration |
Gadgets for identifying consumption patterns and anomalies and for comparing different consumers over time. |
| Energy Analysis Reports Module configuration |
Reports for energy consumption monitoring and modeling, including energy usage by process area or by product output. |
| Energy Billing Module configuration |
Energy-based billing and reporting, including consumption monitoring and reporting at the branch circuit level. |
| Event Notification Module configuration |
Notifications of power system events via email, SMS, or SNMP. |
| Insulation Monitoring Module configuration |
Monitoring for isolated power systems, such as the ones found in hospital operating rooms. |
| Power Quality Performance Module configuration |
Analysis of power quality events and disturbances and their impact on the monitored system. |
Configuration tools and other functions:
| Tool | Task |
|---|---|
| Breaker Configuration Tool | Configure the Breaker Aging Module and the Breaker Settings report. |
| Designer | Configure ION devices and the VIP. |
| Device Manager | Add and manage devices and sites. |
| Device Replacement | Configure processed measurement and device replacement. |
| Device Type Editor | Create device drivers for Modbus and OPC devices. |
| Downstream Device Assistant | Manage downstream devices. |
| Event Watcher Manager | Define events to trigger report subscriptions. |
| EWS Client | Configure the EWS client to import EWS server data. |
| Generator Performance Configuration Tool with EPSS Test Module | Configure the Multi-Source Management Module. |
| Generator Power Configuration Utility | Configure the Multi-Source Management Module. |
| Hierarchy Configuration Utility | Bulk configure Hierarchies. |
| Hierarchy Manager | Configure and maintain Hierarchies, Apportioned Meters, Virtual Meters. |
| Installer | Perform the following tasks: Reconfigure, Reset Accounts, Export System Key, Import System Key, Uninstall |
| Insulation Monitoring Configuration Tool for ANSI | Configure the Insulation Monitoring Module for ANSI applications. |
| Insulation Monitoring Configuration Tool for IEC | Configure the Insulation Monitoring Module for IEC applications. |
| Log Viewer | View system events for troubleshooting and auditing. |
| Logical Device editors | Create logical device types and logical devices. |
| Management Console | Setup the device network, create Managed Circuits, configure Connection Schedules. |
| Manual Data Editor | Manually edit logged measurement data to correct incorrect data or add new data. |
| OPC Server Support | Define which measurements to expose to the OPC server. |
| Power Losses Configuration Utility | Configure the Power Efficiency Module. |
| PQDIF Exporter | Export Power Quality data to PQDIF format. |
| Rate Editor | Configure rates for billing reports. |
| Remote Modem Setup | Configure dialup modems that will be connected to meters at remote locations. |
| Software Logging | Add or edit software based data logging for Modbus device types. |
| System use notification | Set up a system use notification to be displayed before users can log into the system. |
| Time of Use Editor | Define Time of Use schedules for reports. |
| Update EWS Server | Update EWS measurement mappings. |
| Update OPC Server | Update OPC measurement mappings. |
| Upload Report Template | Upload report template |
| UPS Configuration Tool | Configure the Multi-Source Management Module. |
| UPS Power Configuration Utility | Configure the Multi-Source Management Module. |
| User Manager | Configure Users and User Groups. |
| Virtual Processor service (VIP) | Configure the VIP to perform data processing and control functions. |
| Virtual Processor setup | Configure the VIP service. |
| Web Applications settings | Configure Web apps localization, EcoStruxure Web Services Login, Diagnostics and Usage, Report Themes, Alarm Viewer, Annunciator and more. |
References:
| Topic | Content |
|---|---|
| Configuration References | Links to reference information related to the content of the Configuring chapter. |