Web Applications settings
TIP: You can open the Settings page from the SETTINGS link in the Web Applications banner.
Use the Settings page to access web application settings and configuration tools.
NOTE: Access to this application or function is controlled by user privileges.
TIP: Use Search, in the Settings Library, to find the settings and tools you are looking for based on keywords.
The Settings page consists of a Settings Library and a configuration area. The Settings Library provides access to the following settings and tools:
| Category | Settings/Tools |
|---|---|
| Alarms | Alarm Views
Notifications Software Alarms (tool) |
| Personalization | Personal Preferences
Report Theme System Language System Theme |
| Registration & Analytics | Diagnostics and Usage
Registration |
| Security | Diagrams Control Options
Login Options Session Timeout |
| Integrations (Note: This setting is a sub category under Security.) | Authorized Hosts
EWS Client (tool) EWS Server (Note: This setting is hidden when EWS is disabled.) Integration Utility |
| System | Billing Rates (tool) Device Manager (tool) Device Replacement (tool) Hierarchies (tool) Modeling (tool) System Log (tool) |
| Users | User Manager (tool) |
NOTE: The availability of the Billing Rates (Rate Editor) and Modeling are subject to licensing. EcoStruxure Web Services (EWS) Server appears in the Settings pane only if it is enabled in the system.
NOTE: You can customize the web application navigation links (Dashboards, Diagrams, Trends, and so on) in the banner. For example, you can add custom links, hide/unhide/delete links, and re-order links. For details see Customizing the Web Applications links