Deleting a site

Delete a site if this site is no longer needed, for example if all the devices connected to the site have been removed from service.

To delete a site:

  1. In Device Manager, select the Sites tab.
  2. In the sites table, select the row of the site you want to delete, then right-click in the row and select Delete Site in the context menu. This opens the Delete Site confirmation dialog.
  3. In the confirmation dialog box, click OK.

To delete multiple sites:

  1. In Device Manager, select the Sites tab.
  2. In the sites table, select the rows of the sites you want to delete, then right-click in the selected row area and select Delete <number> Sites in the context menu. This opens the Delete Site confirmation dialog.

    TIP: Use Ctrl+Click to select individual sites, use Shift+click to select a block of sites.

  3. In the confirmation dialog box, click OK.

Related topics:

Devices

Sites

Network

For reference information see: