Viewing system device license status
View device license status to verify that the required device licenses are activated in your system. For example, confirm that enough free licenses are available before adding a number of new devices to the system.
notice
LOSS of communication
| ● | Activate product and component licenses prior to the expiry of the trial license. | 
| ● | Activate sufficient licenses for the servers and devices in your system. | 
Failure to follow these instructions can result in loss of data.
To view system device license status:
- In Device Manager, select the Devices tab.
 - Click Options
 in the top right corner of the display pane, and then click View Device Licenses in the options menu. This opens the Device License Information dialog. 
Related topics:
Devices
- Adding a device
 - Editing a device
 - Deleting a device
 - Connecting or disconnecting an Ethernet device
 - Enabling or disabling a device
 - Viewing a device diagram
 
Sites
- Adding a site
 - Editing a site
 - Deleting a site
 - Connecting or disconnecting a site
 - Enabling or disabling a site
 
Network
- Exporting network configuration for use in a different system
 - Importing network configuration from a different system
 
For reference information see:
- Device Manager
 - Device Manager user interface
 - Viewing system device license status