Viewing a device diagram
Device diagrams are device type specific diagrams in the Diagrams application that show historical and real-time data for a device. You can open a device diagram for a device directly from Device Manager.
NOTE: To see data in a diagram, the device must be connected to and communicating with PME.
To view a device diagram:
- In Device Manager, select the Devices tab.
 - In the devices table, select the row of the device for which you want to open the diagram, then right-click in the row and select View Device Diagram in the context menu. This opens the device type specific diagram for this device in a new tab in your browser.
 
Related topics:
Devices
- Adding a device
 - Editing a device
 - Deleting a device
 - Connecting or disconnecting an Ethernet device
 - Enabling or disabling a device
 - Viewing a device diagram
 
Sites
- Adding a site
 - Editing a site
 - Deleting a site
 - Connecting or disconnecting a site
 - Enabling or disabling a site
 
Network
- Exporting network configuration for use in a different system
 - Importing network configuration from a different system
 
For reference information see: