Creating custom diagrams
You create a custom diagram for the Diagrams application with Vista. After you created the diagram, you must add it to the Diagram Library in the Diagrams application to make it available for viewing.
To create a diagram:
- Open Vista and create a new diagram. Use the Vista tools to create display objects and embedded graphics as applicable.
- Save the diagram to
...\
Power Monitoring Expert
\config\diagrams\ud
or any subfolder in this location.
Related topics:
- Configuring Devices diagrams
- Configuring a network diagram
- Creating custom diagrams
- Set default options for a diagram
- Set Diagrams control options
- Diagram Library
- Diagrams registry settings
- Configuring a custom network diagram for direct browser access
- Configuring Power Quality Performance diagrams
- Configuring Power Quality Performance diagrams for multiple sites
For information on how to use Diagrams, see