Configuring Power Quality Performance diagrams for multiple sites
NOTE: These diagrams are part of the Power Quality Performance Module. This Module requires a separate license.
Before you can use these diagrams, you must first configure the Power Quality Performance module. You must complete the following tasks, as part of the Power Quality Performance module configuration for multiple sites:
- Deploy the VIP framework for Power Quality Performance for the sites using Designer.
- Deploy and configure the Power Quality Performance Indicator and Equipment Vista diagrams for the sites.
Related topics:
- Configuring Devices diagrams
- Configuring a network diagram
- Creating custom diagrams
- Set default options for a diagram
- Set Diagrams control options
- Diagram Library
- Diagrams registry settings
- Configuring a custom network diagram for direct browser access
- Configuring Power Quality Performance diagrams
- Configuring Power Quality Performance diagrams for multiple sites
For information on how to use Diagrams, see Diagrams.