Diagram Library
NOTE: You cannot add, edit, share, or delete Devices diagrams. See Configuring Devices diagrams for details.
NOTE: A network diagram is automatically added to the library when it is generated in Vista. See Configuring a network diagram for details.
To add a diagram to the library:
- In Diagrams, open the Diagram Library and navigate to the folder where you want to create the diagram.
(Optional) Add a new folder by clicking Add Folder
at the bottom of the library panel, or by clicking Add Folder in the Options menu
at the top of the library.
- In the Diagram Library, at the bottom of the panel, click the Add Diagram icon
. This opens the Diagram Settings.
- In Diagram Settings, enter a diagram name, select a location, and select the diagram you want to add.
- Save the diagram.
To add a copy of an existing diagram to the library:
- In Diagrams, open the Diagram Library and navigate to the diagram you want to copy.
- Right-click the diagram name or click the Options icon
for this diagram and select Duplicate to create a copy in the same folder. Select Copy To... to create a copy in a different folder.
(Optional) Add a new folder by clicking Add Folder
at the bottom of the library panel, or by clicking Add Folder in the Options menu
at the top of the library.
- (Optional) In the Diagram Library, select the new diagram, right-click the diagram name or click the Options icon
for this diagram and select Edit to open the Diagram Settings. Change the diagram name.
- Save the modified diagram settings.
To edit an existing diagram in the library:
- In Diagrams, open the Diagram Library and navigate to the diagram you want to edit.
- Right-click the diagram name or click the Options icon
for this diagram and select Edit to open the Diagram Settings. Change the diagram name or location.
- Save the modified Diagram Settings.
To share an existing diagram in the library:
- In Diagrams, open the Diagram Library and navigate to the diagram you want to share.
- Right-click the diagram name or click the Options icon
for this diagram and select Share.... This opens the Share Diagram window.
- In Share Diagram, select the user groups you want to share this diagram with.
(Optional) Specify a name for the shared diagram. The groups you are sharing this diagram with will see this name. The name of the original diagram remains unchanged.
- Click OK to share this diagram.
NOTE: When you share a diagram with another user group, it appears in the Shared folder of this group. You cannot share a shared diagram.
To move an existing diagram to a different location in the library:
- In Diagrams, open the Diagram Library and navigate to the diagram you want to move.
(Optional) Add a new folder by clicking Add Folder
at the bottom of the library panel, or by clicking Add Folder in the Options menu
at the top of the library.
- Right-click the diagram name or click the Options icon
for this diagram and select Move To.... This opens the Select Location window.
- In Select Location, select the location you want to move this diagram to.
- Click OK to move the diagram.
To delete a diagram from the library:
- In Diagrams, open the Diagram Library and navigate to the diagram you want to delete.
- Right-click the diagram name or click the Options icon
for this diagram and select Delete
- In Delete Content, click Yes, to delete the diagram from the Diagram Library.
Related topics:
- Configuring Devices diagrams
- Configuring a network diagram
- Creating custom diagrams
- Set default options for a diagram
- Set Diagrams control options
- Diagram Library
- Diagrams registry settings
- Configuring a custom network diagram for direct browser access
- Configuring Power Quality Performance diagrams
- Configuring Power Quality Performance diagrams for multiple sites
For information on how to use Diagrams, see