Set default options for a diagram
NOTE: For each user, Set as my default supersedes Set as system default. For example, if a user with supervisor-level access sets a diagram as the system default diagram, and another user sets a different diagram as their default diagram, that user's default diagram takes priority over the system default diagram, but only for them.
To set the default options for a diagram:
- In Diagrams, open the Diagram Library and navigate to the diagram you want to set as default.
- Right-click the diagram name or click Options
for this diagram and select Set as default to open the Configure Default Item dialog.
- Turn on one or both of Set as my default and Set as system default.
- Click OK to save the modified Diagram Settings.
Related topics:
- Configuring Devices diagrams
- Configuring a network diagram
- Creating custom diagrams
- Set default options for a diagram
- Set Diagrams control options
- Diagram Library
- Diagrams registry settings
- Configuring a custom network diagram for direct browser access
- Configuring Power Quality Performance diagrams
- Configuring Power Quality Performance diagrams for multiple sites
For information on how to use Diagrams, see