Configuring Devices diagrams
Devices diagrams are device type specific diagrams for each configured device in the system. Devices diagrams are created automatically when a new device is added to the system.
NOTE: You cannot delete Devices diagrams.
NOTE: The device type specific diagrams are the same as the ones used in the default Vista network diagram.
NOTE: It takes time for the system to generate the diagrams when you add a new device. Restart Diagrams after adding a new device to see the new device diagrams.
Related topics:
- Configuring Devices diagrams
- Configuring a network diagram
- Creating custom diagrams
- Set default options for a diagram
- Set Diagrams control options
- Diagram Library
- Diagrams registry settings
- Configuring a custom network diagram for direct browser access
- Configuring Power Quality Performance diagrams
- Configuring Power Quality Performance diagrams for multiple sites
For information on how to use Diagrams, see