Reports configuration
TIP: You can open Reports from the
Use the Reports application to generate historical data reports. The reports are saved in the Report Library. PME comes with many default report templates. Use these default templates to create new reports or upload your own custom templates. Set up subscriptions to automatically generate and distribute reports based on a schedule or an event.
warning
inaccurate data results
| ● | Do not incorrectly configure the software or the devices. |
| ● | Do not base your maintenance or service actions solely on messages and information displayed by the software. |
| ● | Do not rely solely on software messages and reports to determine if the system is functioning correctly or meeting all applicable standards and requirements. |
| ● | Consider the implications of unanticipated transmission delays or failures of communications links. |
Failure to follow these instructions can result in death, serious injury, equipment damage, or permanent loss of data.
For information on how to configure the Reports application, refer to the following topics:
Reports:
- Setting Reports prerequisites
- Meeting individual report requirements
- Adding a new report
- Copying a report
- Editing a report
- Moving a report
- Deleting a report
- Sharing a report
Subscriptions:
Other
- Changing the Reports theme
- Uploading a Report Template
- Configuring the Energy Modeling report
- Reports UI
For information on how to use Reports, see Reports.