Deleting a user
Delete a user if this user is no longer needed, for example if someone no longer needs access to PME.
NOTE: Windows users or groups are only removed from PME. The group or user is not deleted from Windows.
NOTE: When a user is deleted, this user will be logged out automatically by the system after a short period of time, if they are logged in.
To delete a user:
- In User Manager, select the Users tab.
- In the users table, select the row of the user you want to delete, and then click Delete  in this row. in this row.
- In the confirmation dialog box, click Delete for a standard user, or Remove for a Windows user or group.
Related topics:
Users
- Users
- Adding a standard user
- Adding a Windows user
- Adding a Windows group
- Changing a username
- Changing a user password
- Changing a user access level
- Changing user details
- Deleting a user
User groups
- User Groups
- Adding a user group
- Adding a user to a user group
- Adding sources to a user group
- Changing a user group name
- Removing a user from a user group
- Removing sources from a user group
- Changing application access for a user group
- Moving a user between user groups
- Deleting a user group
For information on the Web Application user licenses, see:
For information on related Web Application settings, see:
To customize user access level privileges, see:
For reference information see: