Organizing Objects
When organizing objects in a graphic there are many options. You can move, align, arrange, and distribute objects in the work area. You can use the tools on the toolbar or any of the features available from the panes.
For more information, see the following sections: