Actions Associated with Channels on Advanced Drivers
The channels on advanced drivers support a combination of these actions:
- Acknowledge Alarms
- Acknowledge with Comment
- Alarm Response
- Disable Alarms
- Disable Channel
- Disable Comms Logging
- Disable IO Logging
- Disable Telnet
- Disable TLS Logging
- Enable Alarms
- Enable Channel
- Enable Comms Logging
- Enable IO Logging
- Enable Telnet
- Enable TLS Logging—(Channels on which TLS is enabled and configured)
- Release Exclusive Control—(Systems on which Exclusive Control is enabled)
- Remove Alarms
- Remove with Comment
- Reset Call Statistics—(PSTN channels only)
- Reset Outgoing Call Quality Factor—(PSTN channels that are selected for use by call quality factor)
- Reset Serial Port Statistics—(Channels that have Serial connections)
- Reset Statistics
- Take Complete Exclusive Control—(Systems on which Exclusive Control is enabled)
- Take Partial Exclusive Control—(Systems on which Exclusive Control is enabled)
- Unacknowledge Alarms
- Unacknowledge with Comment.
NOTE: The options Delete Interface Event, Log Interface Event, Modify Interface Event, Refresh Alarms, and Reprioritize Alarms are also available from the Edit Action, Edit Method, and Pick Action Configuration windows. These options are methods, not pick actions, and are purely for use with the Automation Interface. For information, see the database Schema.
Further Information
‘Core’ pick actions that are common to many database items: see Object Menu Options in the Geo SCADA Expert Guide to ViewX and Virtual ViewX Clients.
For information on any channel-specific actions that are not listed above, see the relevant driver guide.