Status Attributes Associated with Channels on Advanced Drivers
The channels on advanced drivers support a combination of these status attributes:
- Id
- Full Name
- Type
- Position
- Created—(New channels only)
- Last Modified
- Configuration Change CRC—(Only displayed if this feature is enabled on your system)
- Exclusive Control User—(Only channels that are under Exclusive Control)
- Alarm State
- Alarm Last Updated
- Scan Status Alarm—(Channels on some advanced drivers)
- State Alarm
- Alarm Count
- Suppression Status—(Channels on which Alarm Suppression is configured)
- Suppressing Parent—(Channels on which alarms are currently suppressed)
- Source
- State
- Last Updated
- Quality
- IO Logging
- Serial Port Statistics—(Channels with serial connections only)
- TLS Logging
- Comms Logging
- Telnet
- Comms Statistics
- Message Count
- Scan Quality—(Direct channels only)
- Incoming Calls—(PSTN channels only)
- Outgoing Calls—(PSTN channels only)
- Outgoing Call Quality Factor—(PSTN channels that are selected for use by their call quality factor).
For information on channel status attributes that are not listed above, see the driver-specific documentation.