Insulation Monitoring Module configuration

warning

inaccurate data results

Do not incorrectly configure the software or the devices.
Do not base your maintenance or service actions solely on messages and information displayed by the software.
Do not rely solely on software messages and reports to determine if the system is functioning correctly or meeting all applicable standards and requirements.
Consider the implications of unanticipated transmission delays or failures of communications links.

Failure to follow these instructions can result in death, serious injury, equipment damage, or permanent loss of data.

 

NOTE: This module requires a separate license. See Licensing for more information.

The Insulation Monitoring Module provides monitoring for isolated (IT) power systems, such as the ones found in hospital operating rooms. It also helps in locating isolation faults. The module can be configured for applications based on the IEC standard, and for applications based on the ANSI standard.

The following report and diagrams are part of this module:

  • Insulation Monitoring Report
  • Facility Summary Vista diagram
  • Areas Summary Vista diagram
  • Area Details Vista diagrams

To use the report and diagrams in this module, the module must be configured, and the measurement data must be available as historical data logs in the database.

For information on how to configure this module for the ANSI and IEC markets, see:

 

Related topics:

Insulation Monitoring Module topics

Other Software Modules