Adding a Schedule
Add a Schedule to be used for controlling when Alarm Rules are active and inactive. The new Schedule will be available in the Select Alarm Schedule selection box in the Add Alarm Rule - Schedule window for a new Alarm Rule, or the Schedule tab in the Edit Alarm Rule window for an existing Alarm Rule.
To add a Schedule:
- Click Add Schedule.
You can access this control in the:
- Schedules tab of the main Software Alarms user interface
- Add Alarm Rule - Schedule window (when adding a new Alarm Rule)
- Edit Alarm Rule > Schedule tab (when editing an existing Alarm Rule)
- Enter a Schedule Name.
- Define the active and inactive days and times of the Schedule.
- Click Save.
Related topics:
- Adding a new Alarm Rule
- Enabling or disabling an Alarm Rule
- Editing an Alarm Rule
- Duplicating an Alarm Rule
- Deleting an Alarm Rule
- Using the Setpoint Calculator
- Adding a Schedule
- Software Alarms configuration
For reference information see: