Editing an Alarm Rule
Edit an existing Alarm Rule to add or remove sources and measurements, or to modify the Alarm Rule parameters such as Active and Inactive conditions.
To edit an Alarm Rule:
- In Software Alarms, select the Alarm Rules tab.
- In the Alarm Rules table, find the row of the Rule which you want to edit, and then click Edit
in this row to open the Edit Alarm Rule window.
TIP: You can also open the Edit Alarm Rule window by double-clicking the Alarm Rule in the table or through the Edit command in the right-click context menu.
- In Edit Alarm Rule, select the tab that contains the settings you want to change.
- Update the settings.
- Click Save.
Related topics:
- Adding a new Alarm Rule
- Enabling or disabling an Alarm Rule
- Editing an Alarm Rule
- Duplicating an Alarm Rule
- Deleting an Alarm Rule
- Using the Setpoint Calculator
- Adding a Schedule
- Software Alarms configuration
For reference information see: