Enabling or disabling an Alarm Rule

Enable an alarm rule to start monitoring the alarm conditions defined in the rule for the linked sources. Disable an alarm rule to stop monitoring the alarm conditions defined in the rule for the linked sources.

To enable or disable an Alarm Rule:

  1. In Software Alarms, select the Alarm Rules tab.
  2. In the Alarm Rules table, find the row of the Rule which you want to enable or disable , and then turn Enabled on or off in this row.

Related topics:

For reference information see: