Using the Setpoint Calculator
Use the Setpoint Calculator to calculate values for the Active
and Inactive
Alarm conditions.
- Click Calculate Values
in the Add Alarm Rule - Details window for a new Alarm Rule, or the Details tab in the Edit Alarm Rule window for an existing Alarm Rule. This opens Setpoint Calculator.
- In Setpoint Calculator, enter a baseline value for the measurement you want to monitor in the Baseline entry field.
For example, for an Over Voltage alarm, assume you enter a baseline value of
480
. - Enter a percentage value in the On Setpoint entry field to calculate when the alarm is set
ON
.Using the voltage baseline of
480
, if you enter a105
as the percentage value for On Setpoint, the calculated value is504
, which displays below the entry field.Initially, the On Setpoint and Off Setpoint entry fields are linked. That is, the value you enter in On Setpoint is automatically duplicated in the Off Setpoint entry field.
- To set a different value for Off Setpoint , click the link button
to disable the linking of the entry fields, and then enter a percentage value in the Off Setpoint entry field.
The off setpoint value is calculated and displays below the entry field. For example, using the voltage baseline of
480
, if you enter95
as the percentage value for Off Setpoint, the calculated value is456
, which displays below the entry field. -
Click Apply to add your setpoint values to the respective Active Condition and Inactive Condition fields, or click Cancel to discard your entries and to close the Setpoint Calculator.
Related topics:
- Adding a new Alarm Rule
- Enabling or disabling an Alarm Rule
- Editing an Alarm Rule
- Duplicating an Alarm Rule
- Deleting an Alarm Rule
- Using the Setpoint Calculator
- Adding a Schedule
- Software Alarms configuration
For reference information see: