Deleting an Alarm Rule
Delete Alarm Rules that are no longer needed.
To delete an Alarm Rule:
- In Software Alarms, select the Alarm Rules tab.
- In the Alarm Rules table, find the row of the Rule which you want to delete, and then click Delete
in this row. This opens the Delete Alarm Rule confirmation box.
TIP: You can also delete an Alarm Rule through the Delete command in the right-click context menu.
- Click Delete.
Related topics:
- Adding a new Alarm Rule
- Enabling or disabling an Alarm Rule
- Editing an Alarm Rule
- Duplicating an Alarm Rule
- Deleting an Alarm Rule
- Using the Setpoint Calculator
- Adding a Schedule
- Software Alarms configuration
For reference information see: