Energy Analysis Reports
NOTE: These reports are part of the Energy Analysis Reports Module. This module requires a separate license.
PME includes the following energy analysis report templates:
- Create Model Report
- Duration Curve Report
- Energy Regression Analysis Report
- Energy Usage Per State Report
- KPI Report
- KPI by TOU Report
- Multi Equipment Operation Report
- Power Usage Per State Report
- PUE Summary Report
- Single Equipment Operation Report
- Use Model Report
CAUTION
inaccurate data results
| ● | Do not incorrectly configure the software or the devices. |
| ● | Do not base your maintenance or service actions solely on messages and information displayed by the software. |
| ● | Do not rely solely on software messages and reports to determine if the system is functioning correctly or meeting all applicable standards and requirements. |
Failure to follow these instructions can result in injury or equipment damage.