Mathematical Functions

 

Overview

This part describes the Mathematical function family.

What Is in This Part?

This part contains the following chapters:

oAnalysis: Calculating Integral and Derivative Values

oFrequency_Multiplier: Implementing 32 Blinkers

oFrequency_Output: Implementing a Frequency

oNormalizer_With_Limiter: Scaling the Minimum and Maximum Input

oONE_SEC_PULSE: Providing Pulses Every One Second

oQuantizer: Digitalizing the Input Value for the Interval

oSignal_Saturation: Limiting to Upper and Lower Saturation Limit

oSignal_Statistics: Calculating Maximum, Minimum, Average and Variance

oCheck_Divisor: Checking for Zero Division Condition