Power Quality Performance Module configuration
NOTE: This module requires a separate license. See Licensing for more information.
The Power Quality (PQ) Performance Module analyzes power quality event and disturbance data as well as power factor measurements. It determines the potential impacts of power quality on the monitored power system and displays the results in graphical formats, with color coding to highlight problem areas. The module combines standard software features with specialized components to produce its outputs. The module can also analyzes power quality event and disturbance data as well as power factor measurements based on the hierarchy sites, which are assigned to a user group.
The following reports, diagrams, and Dashboard Gadgets are part of this module:
- Power Quality Impact report
- Power Quality Analysis report
- Power Quality Indicator diagrams
- Standardized Equipment diagrams
- Power Quality Rating gadget
- Power Quality Rating Trend gadget
- Power Quality Incident Breakdown gadget
- Power Quality Incident Impact gadget
- Power Quality Incident Location gadget
- Power Quality Impact gadget
- Power Quality Impact Trend gadget
- Power Factor Impact gadget
- Power Factor Impact Trend gadget
To use the reports, diagrams, and Dashboard Gadgets in this module, the module must be configured. The measurement data must be available as historical data logs in the database.
For information on how to configure this module, see Configure Power Quality Performance.
For information on how to configure this module for multiple sites, see Configure Power Quality Performance for multiple sites.
Related topics:
Power Quality Performance Module topics
- Power Quality Performance Module Design
- Power Quality Performance Module configuration
- Power Quality Performance Module operation
Other Software Modules
- Backup Power Module configuration
- Breaker Performance Module configuration
- Capacity Management Module configuration
- Energy Analysis Dashboard Module configuration
- Energy Analysis Reports Module configuration
- Energy Billing Module configuration
- Event Notification Module configuration
- Insulation Monitoring Module configuration