Capacity Management Module configuration
NOTE: This module requires a separate license. See Licensing for more information.
The Capacity Management Module provides generator, Uninterruptible Power Supply (UPS), and general equipment monitoring and reporting. It also includes transformer and UPS loss monitoring and reporting. The losses are reported in terms of energy and cost.
The following reports, diagrams, and tools are part of this module:
Reports | Diagrams | Tools |
---|---|---|
Branch Circuit Power Report |
n/a | n/a |
Equipment Capacity Report | Equipment Vista Diagrams | Generator Performance Configuration |
Generator Capacity Report | n/a | Generator Performance Configuration |
Generator Power Report | n/a | Generator Power Configuration Utility |
Power Losses Report | n/a | Power Losses Configuration Utility |
UPS Power Report | n/a | UPS Power Configuration Utility |
To use the reports and diagrams in this module, the module must be configured and the measurement data must be available as historical data logs in the database.
For configuration information on the different reports, see:
- Configure the Branch Circuit Power Report
- Configure Generator and Equipment Capacity Reporting
- Configure Generator and UPS Power Reporting
- Configure the Power Losses Report
Related topics:
Capacity Management Module topics
- Capacity Management Module Design
- Capacity Management Module configuration
- Capacity Management Module operation
Other Software Modules
- Backup Power Module configuration
- Breaker Performance Module configuration
- Energy Analysis Dashboard Module configuration
- Energy Analysis Reports Module configuration
- Energy Billing Module configuration
- Event Notification Module configuration
- Insulation Monitoring Module configuration
- Power Quality Performance Module configuration