Energy Analysis Reports Module configuration

NOTE: This module requires a separate license. See Licensing for more information.

The Energy Analysis Reports Module includes reports that help you understand energy usage patterns to find energy waste, analyze transformer and circuit capacity and assess energy usage by process area or by product output. Use the energy modeling capabilities in this module, to forecast consumption, identify unexpected changes in your consumption, or identify actual savings as a result of energy management measures.

The following reports are part of this module:

  • Create Model Report
  • Duration Curve Report
  • Energy Modeling Reports
  • Energy Regression Analysis Report
  • Energy Usage Per State Report
  • KPI Gadget
  • KPI Report
  • KPI by TOU Report
  • Multi Equipment Operation Report
  • Power Usage Per State Report
  • PUE Summary Report
  • Single Equipment Operation Report
  • Use Model Report

warning

inaccurate data results

Do not incorrectly configure the software or the devices.
Do not base your maintenance or service actions solely on messages and information displayed by the software.
Do not rely solely on software messages and reports to determine if the system is functioning correctly or meeting all applicable standards and requirements.
Consider the implications of unanticipated transmission delays or failures of communications links.

Failure to follow these instructions can result in death, serious injury, equipment damage, or permanent loss of data.

 

To configure the Energy Modeling report, see Configuring the Energy Modeling report for special configuration information on this report.

 

To configure the PUE Summary report:

  1. Set up the monitoring devices that record the report data. See Supported measurements and devices for details on which measurements are required.

    NOTE: To use the reports in this module, the measurement data must be available as historical data logs in the database.

  2. Install the PUE VIP framework. See Loading the PUE framework into VIP.
  3. Configure the framework. See Configure the PUE framework.
  4. Create logical devices. See Creating Logical Devices.
  5. Open the report template in the Reports Web Application, set the report input parameters, and generate the report.

TIP: For more information on the PUE Summary Report, see Terms and Definitions and PUE Summary Report Calculations.

 

To configure the Energy Analysis Reports Module (except the Energy Modeling report and the PUE report):

  1. Set up the monitoring devices that record the report data. See Supported measurements and devices for details on which measurements are required.

    NOTE: To use the reports in this module, the measurement data must be available as historical data logs in the database.

  2. Open the report template in the Reports Web Application, set the report input parameters, and generate the report.

 

For information on how to use the reports in this Module, see Energy Analysis Reports

Related topics:

Energy Analysis Reports Module topics

Other Software Modules