Deleting a Device, Measurement, and / or Alarm Mapping
Delete a device, measurement, and / or alarm mapping to delete the device, measurement, and / or alarm mapping information. You can delete one or all device, measurement, or alarm mapping at a time using the EWS Client user interface.
TIP: Select Delete All Mapping to delete all the device, measurement, and alarm mapping.
To delete a device mapping using the EWS Client user interface:
- In EWS Client table, select the row of the EWS client for which you want to delete device mapping, and then click Edit
in this row. This opens the Re-configure EWS Client dialog. - In Re-configure EWS Client, select the Device and Measurement Mapping tab.
- In Device and Measurement Mapping, select the row of the device mapping for which you want to delete, and then click Delete
in this row. -
In the confirmation dialog box, click Delete.
NOTE: On device deletion, the associated measurement(s) are deleted.
To delete a measurement mapping using the EWS Client user interface:
- In EWS Client table, select the row of the EWS client for which you want to delete measurement mapping, and then click Edit
in this row. This opens the Re-configure EWS Client dialog. - In Re-configure EWS Client, select the Device and Measurement Mapping tab.
- In Device and Measurement Mapping, select the row of the measurement mapping for which you want to delete, and then click Delete
in this row. - In the confirmation dialog box, click Delete.
To delete an alarm mapping using the EWS Client user interface:
- In EWS Client table, select the row of the EWS client for which you want to delete alarm mapping, and then click Edit
in this row. This opens the Re-configure EWS Client dialog. - In Re-configure EWS Client, select the Device and Measurement Mapping tab.
- In Device and Measurement Mapping, select the row of an alarm mapping for which you want to delete, and then click Delete
in this row. - In the confirmation dialog box, click Delete.
Related topics:
- Configuring EWS Client
- Re-configuring EWS Client
- Deleting an EWS Client
- Disabling or Enabling an EWS Client
For specific information on mapping, see
- Remapping a Device, Measurement, and / or Alarm Mapping
- Deleting a Device, Measurement, and / or Alarm Mapping
- Enabling or Disabling a Device, Measurement, and / or Alarm Mapping
For reference information see: