Disabling or Enabling an EWS Client
Disable an EWS client to remove it from the communication network. For example, disable an EWS client that is out of service. Enable an EWS client that was previously disabled to reconnect it to the communication network. You can enable or disable one EWS client at a time using the EWS Client user interface.
To disable an EWS Client using the EWS Client user interface:
- In EWS Client table, select the row of the EWS client for which you want to disable, and then click Edit
in this row. This opens the Re-configure EWS Client dialog.
- In Re-configure EWS Client, select the Configuration tab.
- In Configuration, turn off the Enabled option.
- Click OK.
To enable an EWS Client using the EWS Client user interface:
- In EWS Client table, select the row of the EWS client for which you want to enable, and then click Edit
in this row. This opens the Re-configure EWS Client dialog.
- In Re-configure EWS Client, select the Configuration tab.
- In Configuration, turn on the Enabled option.
- Click OK.
Related topics:
- Configuring EWS Client
- Re-configuring EWS Client
- Deleting an EWS Client
- Disabling or Enabling an EWS Client
For specific information on mapping, see
- Remapping a Device, Measurement, and / or Alarm Mapping
- Deleting a Device, Measurement, and / or Alarm Mapping
- Enabling or Disabling a Device, Measurement, and / or Alarm Mapping
For reference information see: