Deleting an EWS Client
Delete an EWS client if it is no longer needed, for example if the EWS server connected to EWS client has been removed from service. You can delete one EWS client at a time using the EWS Client user interface.
NOTE: When an EWS client is deleted, the configuration and mapping is also deleted.
To delete an EWS Client using the EWS Client user interface:
- In EWS Client table, select the row of the EWS client for which you want to delete, and then click Delete
in this row.
- In the confirmation dialog box, click Delete.
Related topics:
- Configuring EWS Client
- Re-configuring EWS Client
- Deleting an EWS Client
- Disabling or Enabling an EWS Client
For specific information on mapping, see
- Remapping a Device, Measurement, and / or Alarm Mapping
- Deleting a Device, Measurement, and / or Alarm Mapping
- Enabling or Disabling a Device, Measurement, and / or Alarm Mapping
For reference information see: