Deleting a notification rule
Delete a notification rule that is no longer needed.
To delete a notification rule:
- In Notification Manager, select the Rules tab.
- In the notification rules table, find the row of the rule which you want to delete, and then click Delete in this row. This opens the Delete Notification Rule confirmation box.
TIP: You can also delete a notification rule through the Delete Rule command in the right-click context menu.
- Click Yes to confirm.
Related Topics:
Event Notification Module configuration
Settings
Rules
- Adding a notification rule
- Enabling or disabling a notification rule
- Editing a notification rule
- Deleting a notification rule
Recipients
Templates
Schedules
For reference information see: