Deleting a template

Delete a template that is no longer needed.

NOTE: If you delete a template that is used in a notification rule, the rule changes automatically to using the default template.

NOTE: You cannot delete the default template.

To delete a template:

  1. In Notification Manager, select the Templates tab.
  2. In the templates table, find the row of the template which you want to delete, and then click Delete in this row. This opens the Delete Template confirmation box.

    TIP: You can also delete a template through the Delete Template command in the right-click context menu.

  3. Click Yes to confirm.

Related Topics:

Event Notification Module configuration

Settings

Rules

Recipients

Templates

Schedules

For reference information see: