Editing a template

Edit an existing template to update the information that is included in the alarm notification messages.

To edit a template:

  1. In Notification Manager, select the Templates tab.
  2. In the templates table, find the row of the template which you want to edit, and then click Edit in this row to open the Edit Template window

    TIP: You can also open Edit Template through the Edit Template command in the right-click context menu or by double-clicking the row.

  3. In Edit Template, update the information you want to change.
  4. Click OK.

Related Topics:

Event Notification Module configuration

Settings

Rules

Recipients

Templates

Schedules

For reference information see: