Adding a recipient
Add a recipient to define the contact information for sending alarm notification messages. The new recipient will be available in the notification rule wizard when adding or editing a rule.
To add a recipient:
- In Notification Manager, select the Recipients tab, and then click Add Recipient to open the Add Recipient window.
TIP: Click Duplicate
or use the Duplicate Recipient command, in the right-click context menu, to duplicate an existing recipient. - Enter the following information:
- Recipient Name: The name that is displayed in the recipients table and the Available Recipients list.
- Email Address: The email address used to send email notifications to this recipient.
- SMS Phone Number: The phone number used to send text notifications to this recipient.
- SNMP Server Name: The server name used to send SNMP message notifications to this recipient.
TIP: Click Test to send a test email, test SMS message, or test SNMP message to confirm that your entries are correct and valid.
NOTE: The notification settings for email, SMS, and SNMP must be configured correctly before you can send test messages. See Editing notification settings for details.
- Click OK.
NOTE: You can also add recipients though the notification rule wizard when adding or editing a rule. Use the same process as described in steps 2-3 above.
Related Topics:
Event Notification Module configuration
Settings
Rules
- Adding a notification rule
- Enabling or disabling a notification rule
- Editing a notification rule
- Deleting a notification rule
Recipients
- Adding a recipient
- Editing a recipient
- Deleting a recipient
Templates
Schedules
For reference information see: