Adding a Schedule
Add a schedule to define the days and times when a notification rule is applied. The new schedule will be available in the notification rule wizard when adding or editing a rule.
NOTE: A schedule only has an effect if the associated notification rule is enabled. If the rule is disabled, the schedule is ignored.
NOTE: Schedules are shared across applications. For example, the same schedule can be used for an alarm rule and a notification rule.
To add a schedule:
- In Notification Manager, select the Schedules tab, and then click Add Schedule to open the Add Schedule window.
TIP: Click Duplicate
or use the Duplicate Schedule command, in the right-click context menu, to duplicate an existing schedule. - Enter a schedule name.
- Define the active and inactive days and times of the schedule.
- Click Save.
NOTE: You can also add schedules though the notification rule wizard when adding or editing a rule. Use the same process as described in steps 2-4 above.
Related Topics:
Event Notification Module configuration
Settings
Rules
- Adding a notification rule
- Enabling or disabling a notification rule
- Editing a notification rule
- Deleting a notification rule
Recipients
Templates
Schedules
- Adding a Schedule
- Editing a schedule
- Deleting a schedule
For reference information see: