Adding a template
Add a template to customize the information that is included in the alarm notification messages. The new template will be available in the notification rule wizard when adding or editing a rule.
NOTE: You can customize the notes text and hyperlink text that is included in a message. You cannot customize the alarm details information in the message.
To add a template:
- In Notification Manager, select the Templates tab, and then click Add Template to open the Add Template window.
TIP: Click Duplicate
or use the Duplicate Template command, in the right-click context menu, to duplicate an existing template. - Enter the following information:
- Template Name: The name that is displayed in the templates table and the Message Template drop-down box.
- Note: The text that is included in the email, SMS, or SNMP message, after the alarm details information.
- Link: (Optional) A hyperlink that is included in the email, SMS, or SNMP message, after the alarm details information and after the Note text.
- Click OK.
NOTE: You can also add templates though the notification rule wizard when adding or editing a rule. Use the same process as described in steps 2-3 above.
Related Topics:
Event Notification Module configuration
Settings
Rules
- Adding a notification rule
- Enabling or disabling a notification rule
- Editing a notification rule
- Deleting a notification rule
Recipients
Templates
- Adding a template
- Editing a template
- Deleting a template
Schedules
For reference information see: