Editing a notification rule
Edit an existing notification rule to add or remove recipients, or to modify the notification rule parameters such as alarm view, schedule, or delivery options.
To edit a notification rule:
- In Notification Manager, select the Rules tab.
- In the notification rules table, find the row of the rule which you want to edit, and then click Edit
in this row to open the Edit Notification Rule windowTIP: You can also open Edit Notification Rule through the Edit Rule command in the right-click context menu or by double-clicking the row.
- In Edit Notification Rule, select the tab that contains the settings you want to change.
- Update the settings.
- Click Save.
Related Topics:
Event Notification Module configuration
Settings
Rules
- Adding a notification rule
- Enabling or disabling a notification rule
- Editing a notification rule
- Deleting a notification rule
Recipients
Templates
Schedules
For reference information see: