Editing a schedule
Edit an existing schedule to change the days and times when a notification rule is applied.
NOTE: Schedules are shared across applications. For example, the same schedule can be used for an alarm rule and a notification rule.
To edit a schedule:
- In Notification Manager, select the Schedules tab.
- In the schedules table, find the row of the schedule which you want to edit, and then click Edit
in this row to open the Edit Schedule windowTIP: You can also open Edit Schedule through the Edit Schedule command in the right-click context menu or by double-clicking the row.
- In Edit Schedule, update the information you want to change.
- Click OK.
Related Topics:
Event Notification Module configuration
Settings
Rules
- Adding a notification rule
- Enabling or disabling a notification rule
- Editing a notification rule
- Deleting a notification rule
Recipients
Templates
Schedules
- Adding a Schedule
- Editing a schedule
- Deleting a schedule
For reference information see: