Deleting a schedule
Delete a schedule that is no longer needed.
NOTE: Schedules are shared across applications. Confirm that a schedule is not in use before deleting it.
NOTE: If you delete a schedule that is used in a notification rule, then this schedule is automatically removed from the rule.
To delete a schedule:
- In Notification Manager, select the Schedules tab.
- In the schedules table, find the row of the schedule which you want to delete, and then click Delete
in this row. This opens the Delete Schedule confirmation box. TIP: You can also delete a schedule through the Delete Schedule command in the right-click context menu.
- Click Yes to confirm.
Related Topics:
Event Notification Module configuration
Settings
Rules
- Adding a notification rule
- Enabling or disabling a notification rule
- Editing a notification rule
- Deleting a notification rule
Recipients
Templates
Schedules
- Adding a Schedule
- Editing a schedule
- Deleting a schedule
For reference information see: