Editing a recipient
Edit an existing recipient to update the recipient information such as name, email, or phone number.
To edit a recipient:
- In Notification Manager, select the Recipients tab.
- In the recipients table, find the row of the recipient which you want to edit, and then click Edit
in this row to open the Edit Recipients window
TIP: You can also open Edit Recipients through the Edit Recipient command in the right-click context menu or by double-clicking the row.
- In Edit Recipient, update the information you want to change.
- Click OK.
Related Topics:
Event Notification Module configuration
Settings
Rules
- Adding a notification rule
- Enabling or disabling a notification rule
- Editing a notification rule
- Deleting a notification rule
Recipients
- Adding a recipient
- Editing a recipient
- Deleting a recipient
Templates
Schedules
For reference information see: