Deleting a recipient
Delete a recipient that is no longer needed.
NOTE: If you delete a recipient that is used in a notification rule, then this recipient is automatically removed from the rule.
To delete a recipient:
- In Notification Manager, select the Recipients tab.
- In the recipients table, find the row of the recipient which you want to delete, and then click Delete
in this row. This opens the Delete Recipient confirmation box. TIP: You can also delete a recipient through the Delete Recipient command in the right-click context menu.
- Click Yes to confirm.
Related Topics:
Event Notification Module configuration
Settings
Rules
- Adding a notification rule
- Enabling or disabling a notification rule
- Editing a notification rule
- Deleting a notification rule
Recipients
- Adding a recipient
- Editing a recipient
- Deleting a recipient
Templates
Schedules
For reference information see: