Adding a notification rule
Add a notification rule to receive messages when alarms or incidents happen in your power system.
To add a new notification rule:
- In Notification Manager, select the Rules tab, and then click Add Notification Rule to open the Add Notification Rule window.
TIP: Click Duplicate
or use the Duplicate command, in the right-click context menu, to duplicate an existing notification rule.
- In Add Notification Rule, select the alarm view for which you want to monitor the activity and receive notifications. Click Next.
- Select one or more recipients to receive a notification. Click Next.
TIP: You can add a new recipient to the system by clicking Add Recipient. See Adding a recipient for more information.
- (Optional) Select a notification schedule and the schedule timezone for this notification rule. Click Next.
TIP: You can add a new schedule to the system by clicking Add Schedule. See Adding a Schedule for more information.
- Specify a notification Rule Name.
- Enable or disable the rule.
- Select a message template.
- Set the Delivery Options:
- Enable or disable email notification.
- Enable or disable SMS notification.
- Enable or disable SNMP notification.
- Set which activities in the alarm view trigger a notification.
NOTE: You can choose to only receive notifications when an alarm goes active or a new incident happens.
Or you can choose to receive notifications on all activity.
- Click Finish.
Related Topics:
Event Notification Module configuration
Settings
Rules
- Adding a notification rule
- Enabling or disabling a notification rule
- Editing a notification rule
- Deleting a notification rule
Recipients
Templates
Schedules
For reference information see: