Adding a Schedule

Add a schedule to define the days and times when a notification rule is applied. The new schedule will be available in the notification rule wizard when adding or editing a rule.

NOTE: A schedule only has an effect if the associated notification rule is enabled. If the rule is disabled, the schedule is ignored.

NOTE: Schedules are shared across applications. For example, the same schedule can be used for an alarm rule and a notification rule.

To add a schedule:

  1. In Notification Manager, select the Schedules tab, and then click Add Schedule to open the Add Schedule window.

    TIP: Click Duplicate or use the Duplicate Schedule command, in the right-click context menu, to duplicate an existing schedule.

  2. Enter a schedule name.
  3. Define the active and inactive days and times of the schedule.
  4. Click Save.

NOTE: You can also add schedules though the notification rule wizard when adding or editing a rule. Use the same process as described in steps 2-4 above.

Related Topics:

Event Notification Module configuration

Settings

Rules

Recipients

Templates

Schedules

For reference information see: