Enabling or disabling a notification rule

Enable a notification rule to start receiving messages when alarms or incidents happen in your power system. Disable a notification rule to stop receiving messages for alarms defined in the rule.

To enable or disable a notification rule:

  1. In Notification Manager, select the Rules tab.
  2. In the notification rules table, find the row of the rule which you want to enable or disable, and then turn Enabled on or off in this row.
  3. Right-click the row and select Edit Rule to open Edit Notification Rule. You can also open Edit Notification Rule by double-clicking the row.
  4. In Edit Notification Rule, select the Settings tab and then turn Rule Enabled on or off.
  5. Click Save.

Related Topics:

Event Notification Module configuration

Settings

Rules

Recipients

Templates

Schedules

For reference information see: