Deleting a template
Delete a template that is no longer needed.
NOTE: If you delete a template that is used in a notification rule, the rule changes automatically to using the default template.
NOTE: You cannot delete the default template.
To delete a template:
- In Notification Manager, select the Templates tab.
- In the templates table, find the row of the template which you want to delete, and then click Delete
in this row. This opens the Delete Template confirmation box.
TIP: You can also delete a template through the Delete Template command in the right-click context menu.
- Click Yes to confirm.
Related Topics:
Event Notification Module configuration
Settings
Rules
- Adding a notification rule
- Enabling or disabling a notification rule
- Editing a notification rule
- Deleting a notification rule
Recipients
Templates
- Adding a template
- Editing a template
- Deleting a template
Schedules
For reference information see: