Editing a template
Edit an existing template to update the information that is included in the alarm notification messages.
To edit a template:
- In Notification Manager, select the Templates tab.
- In the templates table, find the row of the template which you want to edit, and then click Edit
in this row to open the Edit Template window
TIP: You can also open Edit Template through the Edit Template command in the right-click context menu or by double-clicking the row.
- In Edit Template, update the information you want to change.
- Click OK.
Related Topics:
Event Notification Module configuration
Settings
Rules
- Adding a notification rule
- Enabling or disabling a notification rule
- Editing a notification rule
- Deleting a notification rule
Recipients
Templates
- Adding a template
- Editing a template
- Deleting a template
Schedules
For reference information see: