Viewing alarms
View Alarm Status to assess the state of the monitored power system and to respond to important events and issues. View Alarm History for root cause analysis and to understand the sequence of events.
To view Alarm Status or Alarm History:
- In the alarm viewer, open an existing alarm status or alarm history view from the view library or add a new View.
 - View the alarm information displayed in the alarms display pane.
(Optional) In the view library, right-click the view name or click Options
, and select Edit to open the view settings. You can also open the view settings by double-clicking the view name. Adjust the  settings for View Type, Priority, State, Sources, and Categories to customize the view if necessary. Save the modified view settings or click Cancel to discard the changes. 
Related topics:
- Viewing incidents
 - Viewing alarms
 - Viewing events
 - Viewing Disturbance Direction
 - Viewing Load Impact
 - Viewing a timeline analysis
 - Viewing Voltage Tolerance
 - Viewing waveforms
 - Acknowledging alarms
 
For reference information see:
- Alarm Operation
 - Incidents
 - Alarms
 - Events
 - Disturbance Direction
 - Load Impact
 - Timeline analysis
 - Voltage Tolerance
 - Waveforms
 - Waveform analytics
 - Alarms terminology
 - Alarms UI
 - Timeline analysis UI
 - Waveforms UI
 
For information on how to configure Alarms, see Alarms configuration.