Viewing a timeline analysis
View a timeline analysis to investigate the sequence of events that occurred during a single incident, multiple incidents, or alarms.
To view a timeline analysis for an incident:
- In the alarm viewer, open an existing incident view from the view library or add a new View.
 - Find the incident  for which you want to view the analysis, and click Open Timeline Analysis 
 to open the timeline window.
(Optional) Edit the view settings for the timeline analysis and save the view for future reference. 
To view a timeline analysis for multiple incidents:
- In the alarm viewer, open an existing Incident view from the view library or add a new View.
 - Find and select the incidents  for which you want to view the analysis.
TIP: Use
Ctrl+Clickto select individual alarms, useShift+clickto select a block of alarms. -  From the  in the Options menu 
 at the top of the alarms display pane, select Open Timeline Analysis on selection. 
To view a timeline analysis for an alarm:
- In the alarm viewer, open an existing alarm history view from the view library or add a new View.
 - Find the alarm for which you want to view the analysis and click Open Details.
 - In the alarm details window, click Timeline Analysis.
 
Related topics:
- Viewing incidents
 - Viewing alarms
 - Viewing events
 - Viewing Disturbance Direction
 - Viewing Load Impact
 - Viewing a timeline analysis
 - Viewing Voltage Tolerance
 - Viewing waveforms
 - Acknowledging alarms
 
For reference information see:
- Alarm Operation
 - Incidents
 - Alarms
 - Events
 - Disturbance Direction
 - Load Impact
 - Timeline analysis
 - Voltage Tolerance
 - Waveforms
 - Waveform analytics
 - Alarms terminology
 - Alarms UI
 - Timeline analysis UI
 - Waveforms UI
 
For information on how to configure Alarms, see Alarms configuration.